|
Compared to the old system, more than double the number of tests can
now be carried out in the new test bay, thanks to extensive, consistent
automation and modular design.
Setup times on the test stands have been considerably reduced by transferring
the work from the test stand to the shop floor.
The successful test stand concept applied in Hall 72A is now being used
as a template when modernizing existing test stands or creating new ones
both in Wolfsburg and in other VW plants.
VW test stands based on the Hall 72A blueprint have now been constructed
around the world, including in plants in
- Polkowice/Poland
- Mlada Boleslav (Skoda)/Czech Republic
- VW Puebla/Mexico
- Changchun (FAW) and Lou Tang (SVW) in China
|