| Control types
- Speed control
- Tractive force control
- Drive simulation (road resistance including gradient, vehicle mass)
- Calibration
- Coast down
- Accelerator position control
Operation
The test rig has a setup mode (lifting ramps, wheel base setting, accelerator adaptation) and can be used in either manual or automatic mode. In the case of manual mode, selection and setpoints are preset on an operator panel (with graphic display). In automatic mode, a PC is used with a WINDOWS user interface that also supports mouse-free operation.
The plug and play card PC with CATSNT is integrated in a common SIMATIC frame with the digital control and the process I/O. Information is exchanged via an internal bus system by short, interference-free routes in the internal format.
Division of the user interface
- operation of the test data
- test preparations
- test execution
- system setting
- password protection
The setpoints can be set optionally:
- via PC keyboard or mouse
- from the drive profile stored on the PC
- externally via sockets by a master system
As well as in the online mask, all analog variables can be parameterized in an additional measured value display (display with limit value monitoring).
In the control type "Drive simulation" a driver terminal can be used to preset the drive profile so that it displays a speed curve on a monitor for the driver in the vehicle to follow. Drive profile processing can be started, stopped, continued or ended with a manual control unit in the vehicle. The mask below shows the whole drive profile at the left of the screen. To the right of it the current drive profile window is shown enlarged. |