Deutsch
Site Map | Contact Us
Home  |  Products and solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
Products
SIMATIC IT Value Proposition
SIMATIC IT Production Suite
SIMATIC IT Intelligence Suite
SIMATIC IT R&D Suite
SIMATIC IT Independent Components
SIMATIC IT for Industry
Services
Success Stories
Partners
 

SIMATIC IT Intelligence Suite

SIMATIC IT Intelligence Suite transforms and unifies real-time, historical and business data collected during production activities from single or multi-plant environments. This diverse set of data can be integrated and related through a configurable data model and optionally used to populate a data store that collects and retains historical data. Manufacturing intelligence provides a ready source for further analysis of information captured from remote locations. These sets of data, prepared in advance, can be accessed for high level analysis using techniques such as OLAP (On Line Analytical Process).

The benefits of manufacturing intelligence are even stronger if its relationship to MES functionality is very tight. SIMATIC IT provides the perfect environment for realizing this synergy between intelligence and execution. Users that collaborate on solutions using manufacturing intelligence tools can immediately take action and initiate production workflows through SIMATIC IT. As the central mechanism for orchestrating manufacturing workflows, the SIMATIC IT Production Suite transforms and coordinates events with actions, providing a framing context for the entire manufacturing cycle.

SIMATIC IT provides integrated manufacturing intelligence enabling a seamless mechanism for incorporating manufacturing data into intelligence solutions. As SIMATIC IT is the source of the majority of manufacturing information, manufacturing intelligence solutions can be incorporated with minimal effort. With built-in S-95 structures and a set of pre-defined industry specific KPI applications, SIMATIC IT manufacturing solutions can be rapidly deployed.

SIMATIC IT Intelligence Suite allows customers to improve overall profitability and effectiveness in manufacturing operations by focusing on several critical, interrelated areas of production. These areas include the ability to better utilize plant assets (such as people, equipment and materials) through a single or multi-site view of overall equipment efficiency. Through the capability of connecting to existing third party manufacturing installations as well as to legacy systems, SIMATIC IT manufacturing intelligence allows customers to safeguard their previous investments.

Furthermore, the modular architecture of the SIMATIC IT enables the customer to pick only those components he really needs to optimize his daily manufacturing and business challenges. This modular application approach allows for incremental installations and affords users the opportunity to pick and choose what functionality they need without the need for "all or nothing" implementations.

The responsiveness and agility that organizations can realize through the application of manufacturing intelligence are proving to be vital attributes for succeeding in the new economy of today. Through SIMATIC IT manufacturing intelligence, manufacturers are revealing new insights into their business and realizing efficiencies in their operations never previously achieved

 

For more informations about SIMATIC IT Intelligence Suite, please visit:
MES Diving Center

 
     
     
     
Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use