SIMATIC IT for Industry
Siemens has over the past one and a half years implemented an elaborated strategy based on three pillars: Product Differentiation, Whole Product through Partnerships and Focus. As a result of the focus pillar of the strategy, several so called industry initiatives have been developed and implemented over the past year.
They cover various segments from the Food & Beverage, Chemicals and Pharmaceuticals to the Discrete industries and allow Siemens to address the market with a solution tailored to the specific customer' needs, thereby offering maximum value. The systematic approach to various industries allows Siemens and partners to confirm its market leadership and expertise in Manufacturing Execution Systems, industry per industry.
SIMATIC IT for Industry targets the following branches:
Discrete which can be divided in:
Automotive, Other Assembly and Electrical Appliances
Siemens can offer several strategies to target these areas: from the Continuous Control of Production Workflows to the Compliance to regulations, from the Non Conformance Management & Defect Detection to the Total and integrated Warehouse Control and to the Resource and Personnel Management.
Mechatronics
In this branch it is important getting new products in short times, but with a continuous attention to meet compliance needs especially the traceability. Siemens can offer particular products especially designed for these needs able to capture the entire product genealogy or skilled to centralize all quality information.
Hybrid
Food & Beverage, Pharma, Tobacco are the subcategories of this section, each one of them encounters more and more specific manufacturing needs but above all, the regulatory and compliance specifications which impose a raising of the products' quality.
Continuous & Chemicals
This industry is subject to a number of requirements aimed at minimizing the release of chemical substances into the environment during manufacturing and processing.
Siemens with its Products manages the business and the production processes in the chemical industry, optimizing and benchmarking performances and supporting brands in reaching their regulatory compliances.
Siemens is the only one with this systematic and elaborated approach, creating value for the customers with specific needs.
Read more about
SIMATIC IT for Industry
|