Our SIMOTION P references certainly include a reference which is close to the requested machine.
Take a look at our references regarding the motion control system SIMOTION P.
IWU Chemnitz, Germany
PROFINET ensures ultrafast safe control
Retrofitting a press control using PROFINET
With this 16-point die cushion control, the SIMOTION P350-3 V4.1.1 – combined with high-speed ET200S HS PN I/Os – is used for the first time on a real press. This project is also a proof of the superior performance of the SIMOTION device featuring short cycle times (16 hydraulic axes, 250µs PN cycle). At present, the P350-3 is the only Siemens controller that can use high-speed I/Os. The consistent use of the SIMOTION technology objects ensures stable machine operation independently of the cycle time.