Deutsch | Italiano
Site Map | Contact | Index
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
[Advanced]
Products & Systems
Drive Technology
Converters
Motors
Engineering Software
PFAD
PFAD Plus takes you to the optimum drive system
NCSD configurator
Drive ES
STARTER Commissioning Tool
Drive Design Tool SIZER
CAD CREATOR
Automation Systems
Communication
SIMODRIVE sensor measuring systems
Safety Integrated
Industry-specific products
Further Topics
Solutions for branches
Machine tools
Services
References
Partner

PFAD Plus takes you to the optimum drive system

Update to version V2.80

Drive dimensioning with PFAD Plus

Use PFAD Plus to dimension three-phase drives with SIMOVERT MASTERDRIVES in the variants "Vector Control" or "Motion Control", including all the related system components.

Example Single Drive

Single drive - example

A drive system consists of the load (machine), a gearbox in some cases, the motor, the power part (converter or inverter and line entry) and other system components (such as brake unit, cables, output reactor, line reactor).

Load:

  • From fan to servo drive
Motor:
  • Standard asynchronous motors, self-ventilated (1LA/1LG motors)
  • Standard asynchronous motors, separately ventilated (1LA/1LG motors, 1PQ motors)
  • Compact asynchronous motors (1PH7/1PL6 motors)
  • Synchronous servo motors (1FK7/1FK6/1FT6 motors)
Configuration:
  • Mains connection voltages: 3 AC 400 V ... 690 V
  • Power range: 0.55 kW ... 2300 kW
  • Compact Plus, compact, built-in and cabinet units
  • Single, group and multiple motor drives
  • 4-Q operation with brake unit, feeder/energy recovery unit or active front end
  • 12-pulse operation with two feeder units and three-winding transformer

Configuration steps with power supply

Possibilities of the drive design

Possibilities of the drive design

Depending on the type of the drive task, PFAD Plus offers various drive design possibilities:

  • Simple applications with load characteristic curves
    • M~n2, M~n, M=const, P=const
    • Axis winder
  • Load cycle for drives with frequently occurring overload; i.e. specification of , Mload(t) and nload(t)
  • Applications
    • Driving gear/hoisting gear
    • Rotating gear
    • Spindle drive
    • Thrust crank
    • Cross cutter
Depending on the required dynamic properties of the application, selection is possible between "Vector Control" and "Motion Control".

Selection criteria

PFAD Plus does not make a global allocation of motor, converter, inverter, brake unit, feeder unit, feeder/energy recovery unit on a catalog basis, selection is rather made on the basis of the load state. In many cases, this results in a more cost-effective combination. Required minimum values will of course be observed. Installation altitude and ambient temperature are taken into account through the corresponding derating curves.

Help

A configuration is processed in specified configuration steps. Each configuration step is executed in a menu-driven way. No entry can thus be forgotten. Verification of all input values ensures faultless configuration. An extensive help system explains all entries and supports the user in selecting a suitable drive configuration for his or her drive task. Existing configurations can easily be converted into a new configuration - merely change the data and save under a different name. A typical configuration can be called for each possible drive configuration, enabling the user to get familiar with PFAD Plus in an easier way. This is of particular interest for beginners. These examples can of course be copied and used for own applications.

Selecting additional system components

PFAD Plus offers a menu-driven selection of all system components that are possible for a specific configuration. These system components are assigned to the configuration steps power supply, load/motor, converter, inverter, output, feeder converter, input. Additional options are possible for cabinet units. In the "output" configuration step, for example, PFAD Plus determines the output reactor that is required when the motor cable exceeds a certain length. The necessary cross-section is determined on the basis of the cable type, the installation method, and the ambient temperature of the motor cable.

System perturbation calculation

To be able to assess the harmonic contents of the feeding mains, PFAD Plus permits the system perturbation at a specific load point to be calculated for an operation with a converter or with a feeder unit plus inverters. The same applies to a 12-pulse operation with two feeder units and a three-winding transformer. Using a simulation program, PFAD Plus determines the time characteristic of the current and voltage values at the primary and at the secondary side. Using a harmonic analysis, the harmonic contents of the currents and voltages at the primary and secondary side are calculated and output up to the 49th harmonic component. These values can directly be compared with the limit values that are permissible according to the individual standards. In addition, PFAD Plus determines the distortion factors of the primary and secondary voltage.

Calculation results of 12-pulse system perturbation

Calculation results of 12-pulse system perturbation

Output / results

PFAD Plus supplies an extensive documentation for each drive configuration that contains all input values, the calculation results, the characteristic curves (such as motor limit curves) together with the load levels, and a parts and ordering list. Depending on the configuration, the specifications of motor, converter, inverter, feeder unit, feeder/energy recovery unit can also be printed. Parts and ordering list and specifications can, via the clipboard, be entered in Microsoft Office applications.

Thermal and dynamic limit values of a servo drive

Thermal and dynamic limit values of a servo drive


Update to Version V2.80

As compared with the PFAD Plus Version V2.70 available since June 2003, the new Version V2.80 offers many improvements and new functionalities. This comprises mainly the following items:

  • Additional rounding feature for traversing/hoisting gear, slewing gear, spindle.
  • cos acceleration option for the cross cutter.
  • Cruss cutter calculation extended to 2 and 4 knives.
  • Graphic display extended by load values Mload(t), nload(t) for applications.
  • Additional column in the order list that can be edited.
  • Check of the max. speed achieved on compact asynchronous motors regarding the activation time.
  • Gear selection option also with load characteristics.
  • DC link compensation in stationary mode.
  • Minimum l/r ratio changed to 2.5 with slider crank.
  • Additional second gear.

In addition, we have corrected some errors.

The update to the new PFAD Plus Version V2.80 is available at no cost for all users having acquired a PFAD Version that was created with the CD-ROM V2.10 resp. the new Setup V2.60-3.

All about PFAD Plus
Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use