mobile fair guide

Interpack 2011 (Packaging Machines) Machine Guide


Telia 8 SFC

Hall: 15, Booth: C46

The machine

Bielloni will exhibit, with live demos, the new Telia 8 FSC , capable of making a complete 8 colour job change in less than 3 minutes with only 7 meters of waste material.

New features:

· 100% print defect control system

· Automatic control of the printing pressures

· triple nozzles and high speed airflow air drying boxes

But the real innovation of this machine is the anilox sleeve and plate sleeve mandrel support system, the internationally patented “FSC system” which allows:

·ultra fast job change

·extremely sturdy supports (170mm is the thickness)

·Positioning of the ball screws in axis to the cylinder rotation centre. This execution maintains a rigid system avoiding vibrations at high speed.



Machine type

Target industry