Deutsch
Site Map | Contact Us | Index
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
[Advanced]
Publications
References
Trade articles
Press Center
Events & Trade Shows
Newsletter

Publications

Up-to-date, international and innovative - in the NewsCenter you can discover a large range of customized solutions and examples from the field. All further publications find it on that
LinkIndustry Automation and Drive Technologies Portal.

References:

So that you´ll know about our capabilities: Take a look at these specific, customer-oriented and finalized projects!
Siemens has further expanded its range with the integration of Loher GmbH and now offers a complete portfolio of explosion-protected drives: from 0.1 kW to 100 MW, with a speed range up to 15,000 rpm also in the megawatt range, as a standard or customized solution and for all applicable ignition protection types in dust and gas atmospheres. more
Variable speed three-phase current systems with frequency converters are also establishing themselves increasingly in the cement industry. They ensure exact processes, reduce the maintenance effort and save energy. more
With about 1200 m/min, converted 72 km/h, the paper races over the rollers, waltzers and winders. To avoid the web tearing at this speed and to guarantee a consistent paper quality, the drives of the new paper machine of the paper and cardboard factory Varel GmbH & Co KG must bring top performance. more

Trade articles:

Stay abreast by reading about product news
and possible solutions
supplied by Siemens!
With three infeed concepts, the Sinamics drive family has the right solution for every application. Infeed of current without mains feedback as the most economical solution for exclusively motorized operation, standard solutions with uncontrolled infeed/feedback unit for occasional generator operation and controlled infeed/feedback unit for particularly high demands on system availability and mains quality. more
The expectation that fuel prices will increase is just one reason of many for the increasing use of fuel-saving variable-speed electric drives on ships and in the offshore sector. The range of applications for variable-speed electric drives extends from the main propeller drive, through bow and stern thruster drives, pumps, fans up to winches. more
Two thirds of the power consumption in industrial installations are caused by electrical drives. Using efficient drive technology can therefore result in substantial savings. more
Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use