2007-11-21
At this year's SPS/IPC/Drives, Siemens Automation and Drives (A&D) is exhibiting the Sinamics G130 compact built-in converter unit with an extended performance range. The modular drive system now covers the power range from 75 kW to 800 kW. The converter is suitable for drive tasks without mains power regeneration for pumps, fans, compressors, extruders, mixers and mills.
more
|
2007-11-20
Siemens Automation and Drives (A&D) has added a high-speed version to its N-compact range of low voltage motors. Thanks to forced ventilation and special rotor design, the motor is suitable for the speed range up to 5000 rpm.
more
|
2006-11-20
Siemens Automation and Drives (A&D) is exhibiting the new built-in units of the Sinamics S120 converter series, featuring liquid cooling, at the SPS/IPC/Drives 2006 trade fair.
more
|
2006-03-03
With Smart Infeed and Active Infeed, Siemens Automation and Drives (A&D) will present two regenerative feedback concepts for the Sinamics drives family at this year's Hanover Fair. The current from regenerative operation of drives is returned to the system.
more
|
2006-03-03
Dr.-Ing. Jürgen Brandes (1961) has been head of the Large Drives Division of Siemens Automation and Drives (A&D) in Nuremberg since the beginning of the year. Dr. Brandes replaces the previous Division Head, Dr.-Ing. Ulrich Feldmann, who has retired.
more
|
2005-04-12
With the Sinamics S120 cabinet modules, Siemens Automation and Drives (A&D) presents a modular cabinet system for multi-motor drives. The Sinamics S120 cabinet modules provide a compact and ready-to-use drive solution, scalable up to a rating of 4.5MW, for use particularly in machines and plants
more
|
2005-04-07
Potential energy savings in electrical drives in the process industry can now be calculated online. The calculation tool Sinasave from Siemens Automation and Drives (A&D) is available for downloading at www.siemens.de/energiesparprogramm.
more
|
2004-10-07
Siemens Automation and Drives (A&D) is expanding its Sinamics S120 modular drive system in the upper output range with components in the chassis format.
more
|
2004-03-04
The Sinamics product range of Siemens Automation and Drives (A&D) has been expanded with the S150 drive converter for demanding drive applications at high outputs.
more
|
2002-07-10
Siemens Automation and Drives (A&D) has developed the new Sinamics G150 converter for high-performance pumps, fans and turbocompressors. Sinamics G150 is currently the quietest and most compact converter worldwide in a standard control cabinet, and supplements the Siemens Simovert Masterdrives control cabinet units.
more
|
previous
|
next
|