Up-to-date, international and innovative - in the NewsCenter you can discover a large range of customized solutions and examples from the field. All further publications find it on that Industry Automation and Drive Technologies Portal.
References:
So that you´ll know about our capabilities: Take a look at these specific, customer-oriented and finalized projects!
Siemens has further expanded its range with the integration of Loher GmbH and now offers a complete portfolio of explosion-protected drives: from 0.1 kW to 100 MW, with a speed range up to 15,000 rpm also in the megawatt range, as a standard or customized solution and for all applicable ignition protection types in dust and gas atmospheres.
more
The city of Anshan in the northeastern Chinese province of Liaoning is known for its steel industry. Angang Iron & Steel Co. is China's third-largest steel plant. This plant is currently being modernized, a process that also involves installing a new blast furnace blower.
more
Copper mining in the Chilean Andes means mining under extreme conditions: severe frosts and extremely deep snow in winter, and great temperature and humidity fluctuations all year round.
more
High efficiency, compactness and reliability - those are the essential features which distinguish permanent magnet excited synchronous machines and which have by now fully established them in smaller drives.
more