|
|
 |
Sm@rtLib HVAC :
Regulating and component modules for heating, ventilation and
air-conditioning systems
|
 |
Sm@rtLib HVAC is a WinCC Premium Add-on in the form of a
block library of regulating and component modules for integrating
applications in the fields of heating, ventilation and air-conditioning
systems developed by the WinCC Specialist AGU.
These libraries are ideal for customers who already deploy SIMATIC
components in their production facilities, which means that they can use
this SIMATIC infrastructure to control the air conditioning components. This
means that you can easily integrate S7-300 controllers in a WinCC
application and reduce costs significantly. A CPU315 can be used in up to 50
process control technology locations with a CPU317 being used in up to 100.
Sm@rtLib-HVAC provides you with a library that many customers already deploy
and which is qualified for pharmaceutical applications according to
FDA-21CFRPart11regulations . Based on the process engineering basic library,
this library offers additional options
|
|

Fig. Screenshot of a HVAC-application
|
|
Functional range: |
|
- summer-winter compensation
- winter drive
- runtime meter
- time switch program
- blocking protection
- closed loop controller
- three-step controller
|
- interconnected controller
- splitrange (heating/cooling)
- additional-exhaust-mixedair valve
- valve control continous
- valve control discontinous
- weighted mean value
- etc.
|
The library comprises function blocks for S7 controller, as well
as faceplates and symbols for WinCC as ActiveX objects. The WinCC
interface can be configured without programming knowledge by
following menues, which reduces engineering efforts.
|
|
Further Information:
| Address |
AGU GmbH
Von-Ketteler-Str.1
D-51371 Leverkusen |
| Telephone |
+49-214-86860-0 |
| Fax |
+49-214-86860-19 |
| E-mail |
info@agu.de |
| Internet |
www.agu.de |
The hyperlinks above refer to other websites or sources
(in the following called "sites"). Siemens has no control over these sites
and therefore cannot be held responsible for the availability,
completeness or faultiness of such sites. Further on, Siemens does not
endorse and is not responsible or liable for any content, goods and
products or other materials on or available from such sites. Any contract
has to be made exclusively between the consumer and the provider of these
sites on the provider's specific business conditions..
|
|
|
|
|
|