Deutsch
Site Map | Contact Us | Index
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
link to related website
Products and systems
Operator control and monitoring devices
Panel PCs
Industrial-LCD-Monitors
HMI Software
SIMATIC WinCC flexible
WinCC flexible Options
SIMATIC Pro Agent
SIMATIC WinCC
WinCC Options
WinCC Add-ons
ACRON 6 for WinCC
Alarm Management
B.Data
DCC Translation Editor
Historian CONNECT ALARM
PM-ANALYZE
PM-CONTROL
PM-MAINT
PM-OPEN EXPORT
PM-OPEN IMPORT
PM-OPEN TCP/IP
PM-QUALITY
ShutDown WinCC
Sm@rtLib HVAC
System diagnostics
WinCC OPC AE Client
WinCC powerrate
Software Update Service
HMI-Complete systems
Customized products
Success stories
Partners

SIMATIC WinCC powerrate:
Power Management System

SIMATIC WinCC powerrate is a WinCC add-on that ensures transparency in energy consumption from the infeed to the load. Energy data is continuously collected, archived and further processed. With an exact knowledge of the consumption profile, it is possible to identify savings potential, optimize your power supply conditions, and hence lower your energy costs. Monitoring the contractual power limits mitigates unnecessary costs and/or penalties and provides you with the capability to approach the power limit closely.
Full integration into WinCC enables problem-free use of the standard interfaces or standard functionalities of WinCC.

Benefits

  • Identification of energy-intensive loads and processes for the purpose of deriving measures for improving power efficiency
  • Comparison of consumption profiles for more efficient processes
  • Optimizing the company according to energy parameters based on an assessment of consumption and costs.
  • Prevents limit overshoot and the resulting additional costsI
Design

SIMATIC WinCC powerrate comprises the following components:

  • Modules for energy data acquisition and processing
  • Faceplates for displaying and processing the energy data
  • Allocation of the energy data to cost centers using Excel macros.
  • Modules for load management (calculation of trend, limit monitoring, release/inhibit consumers
  • Faceplates for display of results and configuration of load management
  • Excel macro for determining the duration line, thus establishing decision base for load management

 

Functionality
  • Energy data acquisition and processing
    Using off-the-shelf modules, energy data can be collected from any Profibus-enabled devices. The data can be available on the modules in the form of counter pulses, counter values, or power values. From this data, the module calculates the power averages and the work values for a specified period. This data is archived in the WinCC tag logging archive. In addition, a limit forecast is extrapolated for each period.
    A sample function (heat calculation) that can be adapted to the needs of the process at any time by means of open interfaces, has been implemented for the purpose of visualizing customized calculations.
    The data from manually read counters can be entered direct into the system and used for further analysis.
  • Presentation of the energy data
    The currently collected energy data is presented as power averages/ work values per time interval. Trend displays enable analysis of archived energy data as well as its representation in tables.


     
  • Further processing of data
    The archived data can be exported directly from WinCC to Excel. Using predefined macros several reports can be obtained:
    • Cost center report
      In this report, the costs are allocated to different cost centers and the costs calculated on the basis of predefined rates. The results are provided as a table or as a bar graph
    • Duration line
      Based on the archived medium power values, powerrate calculates how often a certain medium value has occurred in a predetermined elapse of time. This characteristic shows whether short-term power peaks exis
    The exported energy data can be customized and processed. WinCC can access the data since it is archived in the WinCC archive.
  • Load management
    Contractual power limits (for current typical usage is the 15 minutes power average) must be adhered to, otherwise drastically increased prices or penalties might be imposed. The load management of SIMATIC WinCC powerrate cyclically executes a trend analysis. If the limit is overshot, it will deliver an alarm or a warning, and will also turn off consumers if configured to do so.


    In order to prevent unnecessary switching there are a number of parameters that allow you to adapt the load management to the current process. all of this can be done user friendly on the faceplate. Consumers distributed across several PLCs can be incorporated in the load management by specific AS - AS communication modules.
  • Additional functions
    To prevent the loss of data in the event of a communication fault, the data are temporarily stored in a circular buffer on the SIMATIC S7. To ensure synchronicity with the power supply company, it is possible to evaluate the synchronization pulse from the power supply company.
Further Information:
 
Address

Siemens AG
Industry sector
A&D CD MM1 Technical Assistance
Postfach 4848
90327 Nürnberg
Germany

Phone +49-911-895-5900
Fax +49-911-895-5907
E-mail technical-assistance@siemens.com
Internet www.siemens.de/powermanagementsystem
Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use