SIMATIC Logon- 
Central, cross-plant user management
User management with SIMATIC Logon integrates itself in the safety system and
user management of Windows and in this way meets the FDA requirements .
Key benefits
- Central, cross-plant user management, integrated in Windows User
Management
- High levels of security due to measures on both the
administrator
and user sides
- Integratied in logging procedures of WinCC flexible/Audit
|
When employing SIMATIC Logon you can connect WinCC flexible stations (PC
systems as well as Panels) to a central user management.
The users have not to be setup inside the user administration of each device,
but are administrated centrally at one Log-on-Server. Thus the efforts for user
administration are reduced while security and clearness increase.
Configuration
In a first step the user administration of each WinCC flexible station has to be
configured by adding the following information
- Required user groups and their rights
- Name of the central station where the central user administration is
installed.
The central user administration is configured by using the same names of user
groups. All users are registered here and are assigned to a user group. Every
user defined in a user group of the same name on the central station has access
to the connected WinCC flexible stations.
If the network fails between the central station with SIMATIC Logon and WinCC
flexible station, the operation is handled through a local, predefined emergency
user.
The password aging and the password regulations for the structure of a password
are defined according to the configuration on the central station and then also
apply for all decentrally connected WinCC flexible stations or the respective
users.
The administrator is able to set up new users online as well as block existing
users. SIMATIC Logon also supports electronic signature.
FDA compliance during runtime is guaranteed by several security mechanisms
- Unambiguous identification of each user (Username and password)
- Lockout after several incorrect entries of a password
- Automatic logoff after a predefined time
Licensing
To set up a central user management you need the following licenses
- SIMATIC Logon basic license
- SIMATIC Logon Remote Access-License (for 3 or 10 devices)
according to the number of connected stations you can install several Remote
Access licenses
Additional
information: |
|
|
|