Deutsch
Site Map | Contact Us | Index
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
link to related website
Products and systems
Success stories
...by industries
...by technologies
...by products
Partners
"One device for seven areas"
Mobile HMI with 25 m operating range at SHU

 
The Schwäbische Härtereitechnik Ulm GmbH & Co. SHU operates the world’s
largest pusher-type hardening plant in Ulm. The fully automated plant, built by the world’s leading manufacturer of heat treatment furnaces and plants, Ipsen International in Kleve, is also one of the most modern and flexible of its kind.
As a main operating unit for the plant with a footprint of 70 x 30 m, Ipsen has chosen a
Simatic Panel PC 670 with a 15" touch screen.
To simplify the setup of the conveyor technology and troubleshooting a  Mobile Panel 170 was added to the plants in an almost instant retrofit .
Mobile HMI with 25 m operating range at SHU
It can be connected to or unplugged from one of the seven connection boxes during operation and immediately shows an overview of the respective plant section after booting up the Windows CE operating system.
 


Download of case study, approx. 0.1 MB,  published in advance 2/2005
Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use