8/27/2012 2:10 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, Perhaps the following links might help: how can you set up a connection between a LOGO! 0BA7 and an HMI Panel? how do you integrate an HMI operator panel into a local network? The IP adress of the panel should be the same as in Logo, only the last digit should be different. You can change IP adres of the panel in Control panel of HMI. Best regards, Wizard |
8/28/2012 10:35 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, If I understand it right, you double click on Icon Profinet and nothing happens? Can you open all other icons? Perhaps you will have to perform an OS update with the option "Reset to factory settings" how do you do an operating system update (OS update) on operator panels? Best regards, Wizard |
8/29/2012 9:09 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, Please check your ip adress in Logo!!! Change IP adress in Logo to 192.168.0.1
Here is a link to manual: SIMATIC HMI HMI devices Basic Panels See page 70. how to configure the Panel. Best regards, Wizard |
8/29/2012 10:55 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello, The device should have an unique IP adress and an unique Device name. A device name could be: panel
Panel should be in transfer mode. (Or project is running and remote control is activated) Here is a link how to proceed: how can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? Best regards, Wizard |
Follow us on