Technical Forum

Communication / Networks

Fanuc robot R-J3 controller

Thread Starter: MrBus   Started: 5/1/2012 2:19 PM   Replies: 12

« Previous thread Next thread »
12» Page 1 of 2 (13 items)
  5/1/2012, 2:19 PM
Joined 1/5/2011
Last visit: 6/14/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I am considering connecting my S1200 14 PLC my Fanuc R-J3 controller using tcp/ip
I have used Profibus throughout my career and am now faced with a controller with out a "standard" PB master. I dont wish to add it.
Anyone do it



=== Edited by MrBus @ 5/1/2012 2:29 PM [GMT ] ===


Top
  5/1/2012, 2:51 PM
Joined 7/7/2010
Last visit: 6/17/2013
Posts: 1994
Rating:
Rated: Excellent [4 out of 5 / rated 203 time(s)]. (203) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
I am considering connecting my S1200 14 PLC my Fanuc R-J3 controller using tcp/ip
I have used Profibus throughout my career and am now faced with a controller with out a "standard" PB master. I dont wish to add it.
Anyone do it

If you have your Fanuc's GSD file, you can import it to your portal software, then select it for your project. Then you can select the proper telegram for cyclic communications with the robot.

Helpful? Rate it.
Solved? Post it.
Top
  5/1/2012, 3:14 PM
Joined 1/5/2011
Last visit: 6/14/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I wish to use TCP/IP
Top
  5/1/2012, 3:37 PM
Joined 7/7/2010
Last visit: 6/17/2013
Posts: 1994
Rating:
Rated: Excellent [4 out of 5 / rated 203 time(s)]. (203) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
I wish to use TCP/IP

Understood.  If there is a profinet gsd file, install it into your portal software.

If you want to create your own communications using sockets or something like that, you are blazing a new trail I think.

Helpful? Rate it.
Solved? Post it.
Top
  5/1/2012, 3:47 PM
Joined 1/5/2011
Last visit: 6/14/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I wish to use TCP/IP
Top
  5/1/2012, 4:58 PM
Joined 7/7/2010
Last visit: 6/17/2013
Posts: 1994
Rating:
Rated: Excellent [4 out of 5 / rated 203 time(s)]. (203) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
I wish to use TCP/IP

Understand better than you want to write your own interface.

The tcp/ip communications commands you need to get comfortable with for the S7-1200 PLC:

TSEND_C
RCV_C
TCON
TDISCON
T_CONFIG

Those commands do what you are wishing to use.

Helpful? Rate it.
Solved? Post it.
Top
  5/2/2012, 10:28 AM
Joined 8/31/2010
Last visit: 6/14/2013
Posts: 1267
Rating:
Rated: Outstanding [3.88 out of 5 / rated 106 time(s)]. (106) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
I wish to use TCP/IP

hello MrBus,
Hope this helps you to get an idea - Ethernet Communication: Data Exchange S7-1200 <-> S7-200 (CE-X20)

Like it? Rate it!
Top
Thank you for this post from:
  5/2/2012, 1:30 PM
Joined 1/5/2011
Last visit: 6/14/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for the start.Due to time constraints. I will select the Profinet interface for my first project, then graduate to socket data.  I will still be working on the application. I am typically in favor of off the self solutions but I have many......    more than 12 of the systems and cost will take its toll.
Top
  5/2/2012, 6:46 PM
Joined 8/31/2010
Last visit: 6/14/2013
Posts: 1267
Rating:
Rated: Outstanding [3.88 out of 5 / rated 106 time(s)]. (106) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
Thanks for the start.Due to time constraints. I will select the Profinet interface for my first project, then graduate to socket data.  I will still be working on the application. I am typically in favor of off the self solutions but I have many......    more than 12 of the systems and cost will take its toll.


Hello MrBus,
PROFINET is more easy in my opinion as it needs very little time to configure and more over it is a deterministic and fast communication

Like it? Rate it!
Top
  5/10/2012, 9:46 PM
Joined 1/5/2011
Last visit: 6/14/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
The  R30iA mate controller is not availible in PN.
Has anyone used the KP1200 Profinet to the TCP/IP proto from AB. the KP1200 can comm to the AB tcp/ip, how about the fanuc robot,  it does tcp/ip to a AB controller?


Top
12» Page 1 of 2 (13 items)
Actions