9/8/2011 8:40 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, Your problem is clear But the problem with the S5-timers is they can't be paused. You have to create your own timers by using the clock pulses (if activated in your CPU properties) Attached an example of a homemade timer. Regards, Marcjan Attachmenttimer.pdf (252 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
9/8/2011 9:14 AM | |
Posts: 4 Rating: (0) |
Thanx for quick answer. But im still not at that level of programing, Can i made something with the timers and counters combinations in LED? |
9/8/2011 10:24 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, FUNCTION FC 4 : VOID
ORGANIZATION_BLOCK OB 1
END_ORGANIZATION_BLOCK [/code] AttachmentForum1.zip (92 Downloads) |
Last edited by: Marcjan at: 9/8/2011 10:37 AMAttached program. Last edited by: Marcjan at: 9/8/2011 10:29 AMProblem solved? |
|
This contribution was helpful to2 thankful Users |
9/8/2011 11:05 AM | |
Posts: 4 Rating: (0) |
Ah, wery nice, Thanx I was think that i can solwe that with five timers and counters..... Regards Arpad |
Follow us on