12/9/2010 7:38 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Which version of Step7 do you have? Try to import HW catalog from attachment. Best regards, Hristo Mihalev AttachmentDPAsi.zip (672 Downloads) |
12/9/2010 9:28 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Open hardware configuration->Option->Edit Catalog Profile. Then profile->Import... Update Step7 5.4 to SP5.( Service Pack 5 for STEP 7 V5.4 and STEP 7 Professional Edition 2006). Best regards, Hristo Mihalev |
12/10/2010 5:21 PM | |
Posts: 5822 Rating: (411)
|
Dear Navnag, if you read the delivery release of the Gateway: Delivery release: DP/AS-Interface Link 20E acc. to AS-i V3.0 (6GK1 415-2AA10) you will find the following information: In STEP 7 HWConfig via the hardware catalog entry "DP/AS-i Link 20E Product Version 3" or in third-party systems via the GSD files for 6GK1415 2AA01. (The fourth output of an A/B slave with 4DI/4DO can only be addressed via the GSD file under STEP7 V5.4 SP4.) Best regards J_Bell |
This contribution was helpful to2 thankful Users |
4/20/2011 8:22 AM | |
Joined: 7/13/2009 Last visit: 3/30/2024 Posts: 2 Rating: (0) |
Dear zakir, |
Follow us on