Technical Forum

Communication / Networks

More than one ProfiBus Master NW in one Redundant FO Ring Config

Thread Starter: rajudon   Started: 8/8/2012 11:55 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  8/8/2012, 11:55 AM
Joined 2/10/2010
Last visit: 5/5/2013
Posts: 54
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Is it possible to achieve redundant FO Ring Configuration (using OLM G12), with more than one ProfiBus Master Network? Please see the attached document to get a clear idea of what I meant to say.

regards,
rajudon

Attachment: ProfiBus FO Redundant Ring NW.pdf  (11 Downloads)

Top
  8/8/2012, 12:40 PM
Joined 9/27/2006
Last visit: 5/22/2013
Posts: 3941
Rating:
Rated: Excellent [4.15 out of 5 / rated 619 time(s)]. (619) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello rajudon;
The following FAQ will give you detailed information and configuration hints for the type of network topology you are planning:

How do you set up a redundant optical ring with two OLMs and what LED display behavior is to be expected?

For more threads on the subject, I suggest you use the search function on the forum (look at the top right of this page) using "Profibus redundant ring" as a search term, for example. If you then refine the search by opening the FAQ and Manuals links you will have access to a great deal of recommendations from Siemens Support and forum participants.

Hope this helps,
Daniel Chartier


Top
Page 1 of 1 (2 items)
Actions