Technical Forum

SIMATIC S5 / STEP 5

Step 5 Module

Thread Starter: ashutosh pethkar   Started: 7/6/2012 1:46 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/6/2012, 1:46 PM
Joined 4/9/2010
Last visit: 9/11/2012
Posts: 18
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi , 
    For All.
    I am converting Step-5 system to Step-7 and i have CPU 110. which is most earlier cpu for Step-5
. Alng with i have Timer Module of MLFB no- 6ES5 380-7AA12 and one more module which is used for thmbwheel switches 6ES5-381-7AA11. i dont have any manual for this. 
     Please someone share manual for this three module as well as suggest replacing hardware configuration for same in S7. plc.
Best Regards.
Ashutosh.
Top
  7/22/2012, 2:23 PM
Joined 11/21/2007
Last visit: 5/17/2013
Posts: 539
Rating:
Rated: Excellent [4.04 out of 5 / rated 24 time(s)]. (24) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello pethkarashu

The Hardware time modules of S5-110A can easily be replaced by software timers of S5/S7.
The Timer value could be adjusted from the Front of the timer modules in S5 110A. If adjustment is required in S5/S7, you can consider a HMI for timer adjustment

Here are some links for S5-110A Manuals :

http://support.automation.siemens.com/WW/view/en/21190174

http://support.automation.siemens.com/WW/view/en/21183225

The 380 timer module details are given in section 5.3 of the Programming manual.

Hope this helps

Cheers

Navnag

There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
Page 1 of 1 (2 items)
Actions