Technical Forum

SIMATIC Panel

bit addressing of process variable in KTP600PN using the S7-1200

Thread Starter: mflima   Started: 7/7/2012 12:34 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  7/7/2012, 12:34 PM
Joined 1/24/2008
Last visit: 5/20/2013
Posts: 18
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dears,

my platform is a TIA V11 SP2 Update 3

Related with Addressing types (Basic Panels) in the Help and in the manual it is said:
 ... Single-digit bit numbers are addressed with "/x" or "/0x" (x = bit number)...

I tried to use this feature in a KTP600PN without sucess. Any body has an example with this feature?

Thanks in advance.

MLima

Top
  7/10/2012, 5:40 PM
Joined 9/5/2011
Last visit: 5/24/2013
Posts: 2595
Rating:
Rated: Outstanding [3.83 out of 5 / rated 132 time(s)]. (132) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
mflima wrote:

Related with Addressing types (Basic Panels) in the Help and in the manual it is said:
 ... Single-digit bit numbers are addressed with "/x" or "/0x" (x = bit number)...




Hello,

Can you write where you have read this? Which page?

Tweety
Top
  7/10/2012, 6:46 PM
Joined 1/24/2008
Last visit: 5/20/2013
Posts: 18
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Tweety,
Maybe the answer is in your question.
In fact the sentence appears in the "Addressing in the C.Logix CPU type" section of the TIA Help, which can means that it doesn't apply to my platform.

Thanks.

MLima
 
Top
Page 1 of 1 (3 items)
Actions