Technical Forum

SINUMERIK CNC automation systems

Sinumerik 840d SL >> Assign axis whit HMI Operate 2.7

Thread Starter: gagarin77   Started: 5/25/2012 2:52 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  5/25/2012, 2:52 PM
Joined 6/9/2011
Last visit: 3/8/2013
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello
I am using for the first time 840D SL,  while I have a good experience with  840d PL
after having recognized the various drives must match them to the axes (eg X, Y, Z)
  but on HMI Operate SW 2.7 SP1 HF3 i not find the softkeys.
  On the old HMI (Advanced I find this rather soft)
where is the softkey in sinumerik operate?

Thanks
Top
  5/25/2012, 3:14 PM
Joined 8/4/2009
Last visit: 5/25/2013
Posts: 2319
Rating:
Rated: Excellent [4.11 out of 5 / rated 396 time(s)]. (396) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello....

What problem are you facing in? which key are you looking for ??

Sinumerik operate is just the Software which is like HMI advanced wha you see in Power line machines

May be are you looking starup this?

Check it out and provide me the details.

Regards,
Prakash

Please no technical questions by Private Message(PM), use the FORUM!!!!!
Top
  5/25/2012, 3:47 PM
Joined 6/9/2011
Last visit: 3/8/2013
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I find corresponding tab key  highlighted  in attachement (HMI advanced) in
HMI operate 2.7 (SP1 HF3)
thank

Attachment: Assign_Axis.jpg  (34 Downloads)

Top
  5/25/2012, 3:53 PM
Joined 8/4/2009
Last visit: 5/25/2013
Posts: 2319
Rating:
Rated: Excellent [4.11 out of 5 / rated 396 time(s)]. (396) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello...

If Sinumerik Operate software is installed  in PCU50.3 you can able to see this information. this is not available in Powerline. You can assign the axis by using this softkey automatically your 30130,30240 etc get configured.

Regards,
Prakash

Please no technical questions by Private Message(PM), use the FORUM!!!!!
Top
  5/27/2012, 7:02 PM
Joined 9/19/2010
Last visit: 5/6/2013
Posts: 15
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi

 

You cannot assign axis in HMI Operate, you must have HMI Advanced or Startup tool to carry out this operation automatically.

 

This is a copy-paste from Sales and delivery release:

The Software HMI-Advanced 7.6 SP2 is still required for drive commissioning.52639015
SINUMERIK Operate 2.7 SP1 and HMI-Advanced 7.6 SP2 HF2 can be installed in parallel on a SINUMERIK PCU 50.3 / PCU 50.5. However, only one of the two user interfaces can be started at one time. You can also use HMI-Advanced 7.6 SP2 or the Startup Tool 7.6 SP2 (on SinuCom DVD) for PC/PG for drive commissioning.

 

Best Regards

Tommy

Top
Page 1 of 1 (5 items)
Actions