Technical Forum

MICROMASTER

Communication of MM440 drive by cp341 card with the help of

Thread Starter: SS11   Started: 1/13/2012 9:14 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  1/13/2012, 9:14 AM
Joined 3/8/2011
Last visit: 5/22/2013
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,

I want to communicate MM440 through USS  by cp341 card.
cpu-315-2dp.
Please give some information regarding USS cable and communication should i use the cat5 cable for communication or profibus for MM440 and CP341.
Top
  1/13/2012, 1:45 PM
Joined 10/29/2007
Last visit: 4/24/2013
Posts: 651
Rating:
Rated: Outstanding [3.54 out of 5 / rated 41 time(s)]. (41) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
pls. see the FAQs:

How do I establish a USS connection to a G110?
 -
partial usable for MM4, see also further info of this FAQ. http://support.automation.siemens.com/WW/view/en/39747607 

MICROMASTER 4: USS Protocol Description (usable for all inverter with USS)http://support.automation.siemens.com/WW/view/en/5734889 

Mit freundlichem Gruß / Best regards

Jens S
Top
  2/5/2012, 8:19 AM
Joined 3/8/2011
Last visit: 5/22/2013
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear sir,

i have connected 11+  4- and 8 gnd at my cp card 341.

At MM440 i have connected 29+ 30- and ground.

On my cp card transmit led is glowing but i am not getting any data on drive.

Is it possible to communicate one master and one slave on USS protocol.Please help me out.
Top
  2/5/2012, 3:15 PM
Joined 11/21/2007
Last visit: 5/23/2013
Posts: 539
Rating:
Rated: Excellent [4.04 out of 5 / rated 24 time(s)]. (24) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Sandy

Here are some tips :

a) Check If Communication settings Address, Baud Rate etc in MM440 Drive and in the CP & your Software.

b)  You have not mentioned what software blocks are you using for USS communication.
     Check the communication settings and BCC generation.

   
c) Also you could connect a Serial communication monitoring software like "Docklight" and see if the Telegram being transmitted by the CP341 is what you want. ( Including the BCC )

Hope this helps

Cheers

Navnag



There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
  2/5/2012, 7:00 PM
Joined 3/8/2011
Last visit: 5/22/2013
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanx Dear

I have used FB7 and FB8 blocks.


BCC formation???

Please give me the suggestion.
Top
Page 1 of 1 (5 items)
Actions