Technical Forum

SINUMERIK CNC automation systems

replacement of ballscrew in hydraulic axis

Thread Starter: sagar k.   Started: 4/25/2011 10:39 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  4/25/2011, 10:39 AM
Joined 1/28/2011
Last visit: 4/28/2013
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Sir, This is regarding CNC machine Hydraulic axis. In 840d controller We have ball screw arrangement in X axis & pitch of this screw is 16 mm ( MD 31030- 16mm/rev ), Now we want to replace this ball screw with 10mm pitch. If it’s possible please explain.Awaiting your early response. Thanking you. 
Top
  4/25/2011, 11:28 AM
Joined 7/16/2006
Last visit: 5/24/2013
Posts: 1447
Rating:
Rated: Outstanding [3.47 out of 5 / rated 164 time(s)]. (164) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi

sagar k. wrote:
Sir, This is regarding CNC machine Hydraulic axis. In 840d controller We have ball screw arrangement in X axis & pitch of this screw is 16 mm ( MD 31030- 16mm/rev ), Now we want to replace this ball screw with 10mm pitch. If it’s possible please explain.Awaiting your early response. Thanking you. 


Replace is posible.

Perhaps:
You must additionary reduct you speed.  !    (Please check it)
As example  
maxinal speed  16m/min   with ball screw 16mm.
maxinal speed  10m/min   with ball screw 10mm.
(The Motor and mechanic  must be faster if you want the old speed, possible)



Do you have a measuring System on this axis  ?
If yes, you must additionl change other parameters.


Greatings Karl
 

Karl
Top
Thank you for this post from:
  4/25/2011, 1:37 PM
Joined 1/28/2011
Last visit: 4/28/2013
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
cry
Sir,
Thanks for replay
This ball screw arrangement is used for rotate the absolute encoder, Total ‘X’ axis movement is -14.764 to 100 (114.764 mm), Hydraulic proporational valve is used for cylinder movement & If cylinder moves 16mm linear then encoder rotates one complete revolution (ball screw directly coupled with encoder shaft). Which is the additional parameter wants to be modify  
Top
Page 1 of 1 (3 items)
Actions