Thread Starter: Jochen1955 Started: 10/26/2009 8:53 AM Replies: 31
Good Moring to you all,
Need a small favor. I’m new to WinCC.
1) What is the easiest way to add a “structure tag”.
2) Can you rename a current “structure tag”.
3) Can you delete a “structure tag”.
Regards
Hi Palmerita!If I go to "structure tags" I do have structure in place.The problem is I added extra element in two of the DB under S7.Called "Boiler" and "Drum".Lets take for example only one structure tag.These structure is called "Boiler" under Boiler I have "Boiler1/Boiler" up to "Boiler6/Boiler".If I right click under Boiler I see the old Boiler structure not with the new element added under S7.If I click properties all areas are greyed out. How can I make them active that I can add the last element.Is this possible.For example "Boiler" stucture is as follow:AT_FW RealST_Flow RealTOT-Reset Bool etcAll things here are greyed out.Now Boiler1/Boiler up to Boiler6/BoilerThis poins to the DB number in which CPU with starting DB14 0.0Here the same all things are greyed out.If I rigth click on "Boiler" there is now Delete possible.If I where to delete structure Boiler I would lose sub-set Boiler1/Boiler up to Boiler6/Boiler.I hoop this makes it more clear in a sense.Regards
Hi All,The more look at this project the more I stumble into a brick wall.I did stop WinCC. I then tried to delete structure instance.This is where the problem lies.Pop-UP window.Delete one Object.The selected object is read only or containes read only objects.The deletion procedure has stopped.I went to windows and looked at the WinCC2 project folder. All files are read only.Wanted to change from read-only but stay read only?This is where it ends.I'm off with flue.Regards
I haven't looked at all your screen shots and can't give you any advise atm as I don't have the knowledge for it. I'm really busy atm so I can't offer help for the time being.Kind regards, Appeltaart