4/1/2024 11:16 AM | |
Joined: 3/14/2024 Last visit: 4/10/2024 Posts: 4 Rating: (0) |
Greetings. I am Dusan from Serbia. I am currently working on commissioning a used CNC lathe with a Sinumerik 810D controller. I have some malfunctions, but I can't determine what causes them without looking at the PLC program. I tried to connect to the Step7 through the MPI port on the 810D CPU. I connected an external 24V power supply to the MPI adapter 6ES7972-0CB20-0XA0. Step7 doesn't see it, I guess because it doesn't have Toolbox for 810D. I would like your help with this. I also have a FlopyDisc from the machine with files: VSA.IBN, PLC.IBN; NCK.IBN , HSA.IBN , ANZ.IBN and DATA.MSD. If there is a PLC program here, what needs to be opened in Step7. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/02/2024 08:24:03New subject after splitting Last edited by: Jen_Moderator at: 04/03/2024 03:44:23Headline optimized. |
|
4/3/2024 3:37 AM | |
Joined: 10/17/2007 Last visit: 5/29/2024 Posts: 3992 Rating: (345)
|
you problem is not 'Toolbox" issue. but communication. You did not mention what is you PG or PC with SIMATIC Manager (STEP7).BUT I think you use PC. you need post picture of your PC, (and check if PC have PCIA card slot) I think you cannot use PC adaptor you need use CP5512 kit. as these kind of HW discontinued if you want you can PM me for the source of CP5512
|
Last edited by: nulizhang at: 04/03/2024 11:46:51If you like my comments please |
|
Follow us on