4/3/2024 1:37 PM | |
Joined: 2/10/2015 Last visit: 4/10/2024 Posts: 285 Rating: (1) |
hello everyone, I come here to ask for your help: I have a new TP1500 Comfort display reference 6AV2 124-0QC02-0AX0, I want to transfer an old program from the same TP1500 comfort display into the new one, because on the screen on the old one there is a big black spot which blocks certain things on the screen. the old program was edited with TIA V13 SP1, so I manage to make the online connection with the display and when I start transferring the program to the display, I am asked for adaptation, I I checked the box then loaded but I receive the following errors: Error loading and connection interrupted. I really need your help to understand what is happening and solve the problem. see attached files thank you for helping me AttachmentATTACHED FILE zip.zip (7 Downloads) |
Last edited by: Jen_Moderator at: 04/04/2024 08:25:12Text formatting optimized. |
|
4/3/2024 3:43 PM | |
Joined: 2/3/2022 Last visit: 4/23/2024 Posts: 304 Rating: (27) |
Hi! Which new version are you using? Br! |
4/4/2024 7:53 AM | |
Joined: 7/5/2013 Last visit: 5/16/2024 Posts: 3083 Rating: (505)
|
Hello Franck,
Datatasheet of the 0AX2 says you need at least TIA V14 SP1. Additionally see the following product note please: Adjustment of ambient temperature range: SIMATIC HMI COMFORT PANEL 15" (6AV2124-0QC02-0AX2; 6AV2124-1QC02-0AX2) Engineering: The reworked Comfort Panel 15" (*-0AX2) are spare part compatible to the previous Comfort Panel 15" and are configured with the previous item no. *-0AX1. Regards, Frink |
Pi is exactly three! |
|
Follow us on