2/20/2024 11:38 AM | |
Joined: 2/6/2023 Last visit: 4/29/2024 Posts: 91 Rating: (11) |
Hi, When you start the IPC and press the ESC key you should access the boot options to start the Windows installation through the DVD. If nothing happens, I would first remove all the peripherals connected to the PC and only have the keyboard. You could also remove the battery: https://support.industry.siemens.com/cs/ww/en/view/109822881/119291303051 leave a few minutes and reconnect the battery so that the BIOS values are reset Have a nice day. |
Last edited by: The Helping Hand at: 02/20/2024 13:06:56Text formatting and link optimized |
|
Follow us on