10/9/2023 8:06 AM | |
Joined: 5/22/2013 Last visit: 5/20/2024 Posts: 49 Rating: (0) |
------------------------------------------------------------------------------------------ |
Last edited by: Icoto at: 10/09/2023 08:07:56Last edited by: Jen_Moderator at: 10/09/2023 12:34:49New subject after splitting |
|
10/10/2023 6:51 AM | |
Joined: 5/6/2022 Last visit: 6/10/2024 Posts: 420 Rating: (83) |
Hi Icoto, The SSL-Handshake issue does only appear, if there is some kind of port forwarding implemented when accessing the panel from somewhere in the internet. Please try to change the external port from 5900 to 5910 which has way less traffic. But be aware, if the port is changed from 5900 to 5910 on the external side, you must also call this new port when the connection shall be done. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on