4/16/2024 9:36 PM | |
Joined: 4/16/2024 Last visit: 4/16/2024 Posts: 1 Rating: (0) |
Con que version de software corre el fimware V1.0.1 TIA PORTAL S7-1200 La CPU es el S7-1200. AC/DC/RLy # 6ES7 214-1BE30-0XB0 ¿Hasta que versión podría actualizarla y con qué versión de Software? Tengo instalado el V18 pero no ve la CPU ------------------------------------------------------------------------------------------ |
Last edited by: caio_e82 at: 04/16/2024 21:38:36Last edited by: caio_e82 at: 04/16/2024 21:39:11Last edited by: caio_e82 at: 04/16/2024 21:42:51Last edited by: Jen_Moderator at: 04/17/2024 06:29:11New subject after splitting |
|
4/17/2024 4:37 AM | |
Joined: 3/30/2020 Last visit: 5/3/2024 Posts: 4473 Rating: (936)
|
Step7 V13 is able to still program the V1 firmware. You can use Step7 V13 with the license of Step7 V18. The V13 and V18 can be installed on the same PC and can work at the same time with only one license. The alternative is to update the firmware. For that you will need (a) the firmware update and (b) a Siemens memory card. [LINK: Operating system updates for CPU 1214C, COMPACT CPU, AC/DC/Relay] |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on