Industry Online Support
Technical Forum
5/15/2007 12:38 PM | |
Posts: 15 Rating: (0) |
Ive attached my program, maybe someone can show me the error of my ways! go easy...im just a beginner! Attachment1way.zip (849 Downloads) |
5/15/2007 2:51 PM | |
Posts: 2930 Rating: (432) |
Hi Brettdixon, I have modified your example: Deleted some blocks (B016, B015, not necessary) Deleted Block B032 and negated R from B030 (same function) Deleted Block B002 and changed Block B030 (from 5 to 10 same function then before) Changed I8 >I6 (I8 is connected to a poti on my LOGO!) I checked it with a LOGO!12/24RC and it works well. As it works: Press I1 (text message 1 comes up) Press I3 (text message 2 comes up and Q2 is ON) Toggle I6 (after 10 times Q2 turns OFF and the display Never the less it works like before the modifications. If it does not work with your HW then check the signal from your pulse meter. Regards Helmut Attachment1way_V2.zip (813 Downloads) |
5/16/2007 7:49 AM | |
Posts: 2930 Rating: (432) |
Hi, You are right. A LOGO!230RC requested also 230V AC at the inputs. Regards Helmut |