4/5/2024 1:49 AM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello; Siemens modified the S7-200 v2 CPUs to mke them more attractive to the South-Asian market around 2009, but the harDware is the same between the 2 families (although the CPUs will have slighty different part numbers. Look at the attachment below, taken from the S7-200 System manual, Appendix H. https://support.industry.siemens.com/cs/ca/en/view/1109582 The only problem you will have is with Microwin, the regional settings of the PC you run it on must be set to indian or Chinese, as you have discovered. Here is a bit of information on the subject: Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 04/05/2024 01:51:36 |
|
This contribution was helpful to1 thankful Users |
Follow us on