5/24/2012 7:43 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Well at least for 6ES7212-1BD30-0XB0 latest update is 2.2.0 So I think you might be right about that V3 will be available only with new order code. |
Best regards, |
|
This contribution was helpful to1 thankful Users |
5/24/2012 10:40 AM | |
Joined: 8/31/2010 Last visit: 5/15/2024 Posts: 1510 Rating: (222) |
Hello automatizzando, You point is very much vaild. One more piece of information from the New S7-1200 System Manual - Edition 04/2012- Chapter 4.5.5 "Note You cannot update an S7-1200 CPU V2.2 or earlier to S7-1200 V3.0 by firmware update." |
Like it? Rate it! |
|
5/24/2012 10:48 AM | |
Joined: 8/31/2010 Last visit: 5/15/2024 Posts: 1510 Rating: (222) |
Hello Guys, Excerpt from the S7-1200 system manual (04/2012) - Chapter 11.2.11 Update Firmware The Update Firmware page allows an "admin" user to update the CPU firmware from a file. "Note You can only update S7-1200 CPUs of version 3.0 and higher with the Update Firmware feature." Hopefully this applies for all S7-1200 CPU with FW 3 and above. So Simatic Memory Card is no more mandate for Firmware Updates of FW 3 and above CPUs. The wait is over now. |
Last edited by: Ganes10 at: 5/24/2012 10:50 AMLike it? Rate it! |
|
3/11/2014 10:58 AM | |
Posts: 14 Rating: (0) |
Can I update firmware from V2.2 to V3.0 now? Need I memory card? |