4/13/2018 4:54 AM | |
Posts: 1 Rating: (0) |
Hai Denilson, As i tried to open the Modbus TCP with S7-1500 TIA V14 but i can't open so please help me how to open that TIA V13 file on TIA V14 software. |
4/28/2018 3:38 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424)
|
Hi, sorry but I don't have a V13 version of it. Anyway, Here there are a V15 version of a demonstration program and casts showing about how it was created. The project uses S7-1500 (but the configuration is similar to S7-1200). The use of S7-1500 has the advantage to be simulated in PLCSIM Advanced. The casts could be used as basis to build a project from zero. AttachmentMODBUS.zip (2194 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to5 thankful Users |
8/7/2018 10:55 PM | |
Joined: 8/18/2015 Last visit: 4/13/2023 Posts: 5 Rating: (1) |
Hi, with the internet examples, I made an example project between two s7-1200 (one as a server and the other as a client) maybe it can help you. use version 14 of the TIA PORTAL, CPUs with firmware version 4.2 and MODBUS instructions V4.1. The blocks were without optimized access. regards
AttachmentTestModbusClient_1_20180807_1549.zip (1168 Downloads) |
This contribution was helpful to2 thankful Users |
8/7/2018 11:00 PM | |
Joined: 8/18/2015 Last visit: 4/13/2023 Posts: 5 Rating: (1) |
attachment video example... AttachmentModbus TCP S7-1200 Exe.zip (991 Downloads) |
Last edited by: rojasalmut2 at: 8/7/2018 11:16:48 PM |
|
This contribution was helpful to1 thankful Users |
1/17/2019 10:59 AM | |
Joined: 12/8/2015 Last visit: 4/21/2021 Posts: 2 Rating: (0) |
Hi, Hope the attached program backup would help. |
This contribution was helpful to1 thankful Users |
Follow us on