12/16/2009 3:44 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, which windows operation system do you use????First check the compatibility between SIMATIC NET PC software and operation system. See: http://support.automation.siemens.com/WW/view/en/9859007 |
12/17/2009 3:53 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, SIMATIC NET Edition 2008 HF1 don`t support Server 2003 R2 SP2 Enterprise Edition. Please try to install the SIMATIC NET Software on Standard Server. If you have the same problem than, I recommand tosend a Support Request to the Hotline. Support Request |
12/17/2009 3:55 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Sorry the wrong link... Here comes the right link to Support Request |
3/18/2010 9:30 PM | |
Posts: 42 Rating: (10) |
Problem solved! It wasa problem in s7DOS. |
This contribution was helpful to1 thankful Users |
3/30/2010 7:39 PM | |
Posts: 42 Rating: (10) |
Here is the solution for the problem above: The error is caused by a bug in S7DOS. S7DOS is a component, and cannot be installed separately, but you can install the HF1 of Simatic NET CD 2008 SP2 to solve the problem. You can download the SimaticNet 2008 SP2and it´s HF1 with the following link:SimaticNet 2008 SP2 HF1: http://support.automation.siemens.com/WW/view/en/12660737 SimaticNet 2008 SP2 must be ordered as told in the following link http://support.automation.siemens.com/WW/view/en/40862824 Accordingly to Siemens, this correction will be in the next future HF (HF5) for WinCC V7.0 SP1 too. Personally I think it´ll be necessary to make a WinCC7.0 SP2. Procedure of installation: 1. At first you´ll need to install WinCC7.0 SP1 + SimaticNet Package. When a window is prompted to continue with the installation of Simatic NCM, you will need to manually stop the service s7epatsx.exe in Windows Task Manager, then, you can continue with the installation. 2. Install SimaticNet 2008 SP2 (the one you download through the above link). 3. Install HF1 for SimaticNet 2008 SP2 (again, the one you download through the above link). We have made this procedure here and the server is working well now.If you have any difficult, please don´t hesitate to contact me again. I hope that I have helped you. Have a nice day. |
Last edited by: O_Moderator at: 4/7/2010 11:18 AMlinks edited Last edited by: Gabriel_Rabelo at: 3/30/2010 7:42 PM |
|
This contribution was helpful to4 thankful Users |
3/3/2011 11:24 AM | |
Joined: 2/16/2011 Last visit: 2/3/2022 Posts: 9 Rating: (0) |
Thanks Simens Support Team and Joerg Rennert. The problem simply solved by using correct HF1:ftp.sbs.de/CD2008SP2HF1.zip The HF1 from links listed at top (v7.1.0.1) not valid (not for SP2 i think) |
Last edited by: BETEP59 at: 3/3/2011 11:43 AM |
|