5/24/2012 7:47 AM | |
Posts: 19 Rating: (0) |
by the way im using TIA portal V11 SP2 + WinCC Professional V11 SP2 + CPU1214C |
5/24/2012 11:41 AM | |
Posts: 3037 Rating: (192)
|
Hello, You find more information about server client system of WinCC Professionalin the following manual. See the chapter 9.16.3 WinCC Professional V11.0 SP2 Do you have a HMI connection between your server and your client? See the screenshot. Tweety |
5/25/2012 12:25 PM | |
Posts: 3037 Rating: (192)
|
Hello, Why do younot use a single PC station with Professional Runtime? Why do you use Server andClient on one PC? Tweety |
5/25/2012 9:03 PM | |
Posts: 19 Rating: (0) |
Picture of my network connection |
8/19/2015 9:51 AM | |
Posts: 14 Rating: (2) |
Hello! I've got the same problem. Anybody solve this problem? I cant find any more information about situation, when configuration station and PC station are identical https://support.industry.siemens.com/cs/attachments/77377601/PH_PC-Stations_76.pdf QUOTE: Online mode - local (configuration station and PC station identical) This situation occurs when the configuration system is installed on the PC station (engineering station). In this case, the configuration data is transferred directly over an internal PC connection. Within the configuration system, you still use the known mechanisms for accessing the target system. Follow the steps below: Procedure for the step "downloading project engineering data to the PC station" - online - local Tool 1. Make sure that the following requirement is met: The access point of the application must be set as follows: S7ONLINE (STEP 7) → PC internal (local) STEP 7 Professional (TIA Portal) 2. Select the station you want to download to in the STEP 7 Professional project. STEP 7 Professional (TIA Portal) 3. Download the engineering data with Online → Download to device STEP 7 Professional (TIA Portal). But again and again that message: "Unexpected error during download" "Uploading of device to the same computer is not permitted" Help me please TIA PORTAL V12 |
Last edited by: waard at: 8/19/2015 9:53:00 AMLast edited by: Min_Moderator at: 8/19/2015 11:48:27 AMReplaced link |
|
8/20/2015 8:38 AM | |
Posts: 14 Rating: (2) |
2-nd screen: |
8/21/2015 2:46 PM | |
Posts: 14 Rating: (2) |
help me please, anybody. |
8/21/2015 4:56 PM | |
Posts: 14 Rating: (2) |
Thank you, i read it your answer upside-down, i do it and its work. Big thanks to you! |
Last edited by: waard at: 8/21/2015 5:14:14 PM |
|