11/22/2010 10:59 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello everybody, 30 views so far but not a single reply. Is it so difficult? DEEP. |
12/16/2010 1:14 PM | |
Posts: 7 Rating: (0) |
Dear Deep, |
12/20/2010 1:30 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hi srrr-in, Where shall I get that information. Regards, DEEP |
2/11/2011 3:31 PM | |
Posts: 66 Rating: (4) |
Hello Deep, As an example you could check the "Planning Manual - Planning with SIVACON S8, Flexible Low-Voltage Switchboard", available on http://support.automation.siemens.com/WW/view/en/20356391/133300. Chapter 8.10 provides a table showing short-circuit currents of three-phase distribution transformers.These are maximum values on the transformer output. The longer the cable way from the transformer to your panel the lower this value (impedance of the cable). Regards, Sentronix |
5/23/2012 7:52 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hi, Please find enclosed here with SLD of one of the machine connected named as BETTS lathe. Main SFU is 630 A. For any doubts or information if required, please revert back. DEEP. AttachmentSLD Betts lathe.pdf (344 Downloads) |
6/2/2012 2:35 PM | |
Posts: 12 Rating: (0) |
Good Day, On how to determine the interrupting capacity of the breaker you should cumpute the Isc your network...there is a lot of computation needed to know in interrupting capacity(KAIC). here is the attached file hope that can help you...if you have question and feedback im open to help.... AttachmentCalculation of short-circuit currents.pdf (546 Downloads) |
This contribution was helpful to5 thankful Users |
7/2/2013 7:25 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Hello Deep I was searching from google and found some nice explanation http://mandrelectrical.com.au/karatings.php http://www.electrical-installation.org/enwiki/Selection_of_a_circuit-breaker I think, this will guide you further Hope this will help you Best Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to4 thankful Users |
7/2/2013 7:46 AM | |
Posts: 262 Rating: (45) |
Hi, In Siemens, we recommend to use the best way of calculating Fault level and that is SIMARIS Software... please refer the below link and download it freely and use extensively... https://www.automation.siemens.com/mcms/electrical-design-software/en/service-support/simaris-software/Pages/default.aspx |
This contribution was helpful to1 thankful Users |
7/17/2013 1:48 PM | |
Posts: 202 Rating: (16) |
Hi There Can any tell me how the Fault level for transformer is decided as from that fault level the PCC & MCC panel are designed ???
|