11/18/2009 1:17 AM | |
Posts: 51 Rating: (3) |
hello... wondering if anyone had any experiences good/bad at trying to install STEP7 on Windows 7 Professional (64-bit edition)? I tried to follow some instructions i found for doing it on 32-bit windows http://xuek.ru/eblog/2009/10/step7-at-win7/ but it did not work. i modified the .msi files to allow me to ignore the OS version, and copied the Common Files\Siemens folder to the appropriate location but the install process ditches with a pretty non-specific error (something along the lines of "not all programs were installed") not the end of the world if it's not possible as i have another machine i can get up and running for it, would just have been nice to get it working on my new laptop |
3/8/2010 5:57 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello tomearp, Look at http://www.microsoft.com/windows/virtual-pc/download.aspx Best regards, Hristo Mihalev |
1/5/2011 4:58 PM | |
Joined: 4/8/2008 Last visit: 4/22/2024 Posts: 31 Rating: (2) |
For the network issue; in your virtual machine management area open it's settings and under networking select your network card as a connection. You then must setup your network configuration under the XP machine as you normally would. To get around the remote desktop issue I installed the free version of Real VNC but VNC client/server combination should work. Tiny VNC and Tight VNC are other options. I installed the client and server on each but you need the server on the XP Mode machine and the Client on the Windows 7 machine. |
Glenn |
|
1/6/2011 3:57 PM | |
Posts: 4 Rating: (0) |
Thank you, that has sorted that part and is now fully installed. Patrícia |
1/6/2011 3:59 PM | |
Posts: 4 Rating: (0) |
Thank you!! That worked wonders. It is now installed and working. Patrícia |
2/5/2011 10:56 AM | |
Posts: 54 Rating: (0) |
bit of a bump... can we run Step 7 on our W7 64bit machines yet?? |
3/18/2011 7:17 PM |
|
Posts: 54 Rating: (0) |
Bump again. I have V5.5 for Windows 7 32bit. Any news on 64 bit?? |
Follow us on