11/30/2010 6:34 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Did you check in : STEP 7 Fehlercodes (English) if some of remedies there could helps. Best regards, Hristo Mihalev |
11/30/2010 3:05 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Greg, there is no way,
More at Innovated ET200S IM151-8(F) PN/DP CPU V3.2 Released for Delivery Try to put in hardware configuration the newer type CPU and download... Just check the result... Best regards, Hristo Mihalev |
12/1/2010 1:52 AM | |
Joined: 10/7/2005 Last visit: 5/5/2024 Posts: 3004 Rating: (1046)
|
Hello ggs24 you said you checkedthe Step 7 Error coderemedies for error 294:23 as per UMENCHO's original advise and did not find anything "obvious". I wonder though if you considered and verified thevalid range of DB's, FC's, FB's etc. for your 6ES7151-8FB00-0AB0CPU as per its technical specification. I suggest you check again what numbers of Safety related DB's, FC's, FB's you actually haveas gut feeling tells me you are using DB numbers above the max permissible 511 foryour CPU. Note too the max local data which is 511 Bytes for your CPU. If this is in fact the case (I am somewhat guessing here), you will either have to change the Safety user program and/orchange the "F-Parameters" configuration in the CPU's properties (HWconfig) to avoid that the safety program compilation can create SafetyBlocks whose number is outside the CPU capabilities. Please also change the CPU configuration back to what you orignally had (configure as a 6ES7151-8FB00-0AB0FW V2.7 in HWconfig). Let us know what you'll find and if the above is not applicable in your case, it would help if you could upload your S7 project here. |
Cheers |
|
12/1/2010 2:34 PM | |
Joined: 11/17/2010 Last visit: 4/18/2024 Posts: 26 Rating: (0) |
Fritz, AttachmentTest2.zip (213 Downloads) |
12/2/2010 1:57 AM | |
Joined: 10/7/2005 Last visit: 5/5/2024 Posts: 3004 Rating: (1046)
|
Hello ggs24
Iwould ignore this, these access rights are for the standard user program, Safety has (demands) itsown password protection.
Untick "Support device replacement without exchangeable medium" in the properties of the CPU's PN port (HWconfig) and this problem shouldgo away. As for the test program I noticed a few things: Good: - Your F-Parameters lookok (Numbers are within therange of the CPU) Not so good: -What's the safety password (I can only look but not compile and test without it)? -Your test configuration is not complete, e.g. the F_Call is missing and theconfiguration of the theF-Runtime group is not complete Can you try the following: 1.) Clear the MMC of the CPU with a PG (to make sure there's no leftover stuf in it) 2.) Complete the Safety test configuration (with F_Call and F-Runtime group) and try again If you have still issues afterwards, upload the test configuration here again and let us know the passwords for the safety program. Ihope this helps |
Cheers |
|
12/2/2010 1:44 PM | |
Joined: 11/17/2010 Last visit: 4/18/2024 Posts: 26 Rating: (0) |
Fritz, Thanks for your response. I did everything you asked. I first unchecked the "Support device replacement..." checkbox to retain the the IP address and recompiled hw. I then proceeded to complete the F-runtime group and F-Call and completely compiled the safety program. I even added the cyclic interrupt and call to the F-call.Safety program compiled and consistent. I then removed the old MMC from the CPU, performed a CPU memory reset, and inserted a "brand new" MMC (512k), and downloaded the config (I do not have adevice to erase MMC). I tried to download safety program - same error message. I then cycled power to the CPU - IP address reset again. Is my CPU defective or am I still missing a step somewhere? Please see attached program. Safety password is 'foriauto'. CPU password is either 'fori' or 'fori1'. Regards, Greg AttachmentTesting2.zip (176 Downloads) |
11/16/2015 10:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by codza is split to a separate thread with the subject IM151-8F PN/DP, how i can monitor my profisafe inputs and outputs?. Best regards |
Follow us on