1/12/2007 8:31 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, May be there is some hope,I found some information about a USB to PCMCIA converter. |
Smurf |
|
1/12/2007 8:49 PM | |
Posts: 324 Rating: (30) |
Hi Smurf, have you read the content of the Page? There it is written that only all 16 PC Cards are supported, but the 32 Bit Cardbus Cards are still under development, see for yourself: "This can be any standard or custom 16-bit PCMCIA card (Type I, II, or III). Just for your information the CP 5512 is a Cardbus Adaptor.... only a CP 5511 is a PCMCIA Card (16 Bit). Best regards Calm_down |
4/26/2007 5:02 PM | |
Posts: 7 Rating: (2) |
Hi there, As it seems, the following adapter works fine. Also on PROFIBUS slave modules. http://www.duel-systems.com/products/CategoryDatasheet.aspx?id=4 |
9/22/2007 4:30 PM | |
Posts: 115 Rating: (1) |
Dear Michaelk, If your operating system recognize the USB-PCMCIA adapter ,in my mind it should work and you can use CP5512. Saeed |
9/23/2007 10:45 AM | |
Posts: 7 Rating: (2) |
Hi there! USB can do the job but as far as I know, you cannot connect to PROFIBUS slaves! As we all know the 5512 is the perfect card to programm with. I have found a simple solution: http://www.duel-systems.com/products/adapters.aspx It works fine, not very expensive!!! use it! Not plug & pray, it really works |
9/24/2007 9:23 AM | |
Posts: 324 Rating: (30) |
Hi there, isn't it funny... I do not see anything with USB there... only Express Card, strange isn't it. Stay calm. |
11/24/2008 2:06 PM | |
Joined: 12/6/2006 Last visit: 3/27/2024 Posts: 90 Rating: (0) |
Dear mamssass, U can use CP5711 Card Please find the Details of the card with the attachment AttachmentCP5711.pdf (440 Downloads) |
Last edited by: CS Moderator at: 11/24/2008 5:04 PMpersonal data from a siemens employee deleted |
|
11/28/2008 6:11 PM | |
Posts: 19 Rating: (0) |
Hi everyone, I have just bought a Notebook HP Compaq 6730b (it has serial port RS232C; OS XP Professional SP3) and DuelAdapter. It works with CP5512 properly (CP5512 (PPI) with MicroWin and S7-200 so far). Only one problem is, that I have to insert DuelAdapter with the CP5512 after switch-on of the Notebook. When I switch-on Laptop with DuelAdapter inserted, CP5512 is not activated. I am going to test this configuration with WinCC Flexible and TP177B panel next week. I have problem with an WinCC Flexible installation (SQL Server installation failed). V.Slovak Thevia company Czech Rep. |
12/8/2008 5:22 PM | |
Posts: 19 Rating: (0) |
Hi, I have problem with MPI a DP protocol; CP5512 + DuelAdapter + HP 6730b does'nt work with panel TP170B Mono. I am going to try connection again, but just now I have a lot of work. There is not problem with S7-200 (CPU226) and protocol PPI. V.Slovak Czech Rep. |
Follow us on