7/5/2013 10:56 AM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
BLKMOV in SCLSolution from Smiffy: [code]FUNCTION_BLOCK FB12 Best regards Hamid Hosseini |
This contribution was helpful to3 thankful Users |
7/5/2013 1:51 PM | |
Posts: 55 Rating: (0) |
Dear hdhosseini, Thanks for the quickanswer. It worked well... Thank you so much. Regards, Prasad |
2/17/2014 7:47 PM | |
Posts: 340 Rating: (6) |
new question is splittet to Do you have this code but then for a s7-1200 plc (1214C). |
10/21/2014 4:02 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
11/5/2014 6:34 PM | |
Posts: 3 Rating: (0) |
The rest of code is copied from the previous posts. But when CPU executes the code, no data are copied. So I just wanna know if the definition of pointer is correct. I used the start of the DB (0. byte), because there is no way to make a mistake with addresses. I dont now now where is the problem.
AttachmentSCL Source.pdf (363 Downloads) |
Follow us on