12/13/2022 4:38 PM | |
Joined: 4/23/2015 Last visit: 6/9/2024 Posts: 9 Rating: (0) |
After copy the sdblocks to project , compile err. I have did the option - block type , update Import Libraries to V620. |
12/14/2022 7:27 AM | |
Joined: 4/23/2015 Last visit: 6/9/2024 Posts: 9 Rating: (0) |
The setting follow the attachment. I guess maybe the SMATI5.msk err cause all the logs. |
12/14/2022 10:25 AM | |
Joined: 8/25/2006 Last visit: 6/11/2024 Posts: 2207 Rating: (278)
|
It will be better to ask the customer wich SW versions are used on him PC and install the same. |
12/14/2022 10:41 AM | |
Joined: 4/23/2015 Last visit: 6/9/2024 Posts: 9 Rating: (0) |
After the operation step , err change ,attached the log file. I guess the SMATI5 is a 3rd Lib by Supplier defined。 Attachmentcompile err log.pdf (517 Downloads) |
12/14/2022 12:57 PM | |
Joined: 8/25/2006 Last visit: 6/11/2024 Posts: 2207 Rating: (278)
|
Yes, you need D7-SYS V7.0 HF1 or HF2. |
Follow us on