Industry Online Support
Technical Forum
10/29/2014 4:29 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Usually there is a symbol showing AC or DC on the devices. Normally AC Coils should also carry the rated frequency e.g. 50 / 60 Hz. A Coil without the freq. specification is likely to be a DC Coil. For DC Coils, you can check the resistance with a Multimeter, it should be 24/1.61 ( Apprx 15 Ohms ) Ohms The attached application note may be of interest to understand the differences. Hope this helps Cheers Navnag AttachmentOperating_DC_Relasy_from_AC_and_Vice_Versa_13c3250.pdf (597 Downloads) |
Last edited by: Navnag at: 10/29/2014 6:08 AMAttachment added There is no such thing as the last bug in a program |
|
Follow us on