12/5/2011 11:19 AM | |
Posts: 54 Rating: (1) |
Hello, I'm search example project 'Texas instruments 545-1106 cpu master-->cpu315 2pn/dp slave profibus communication. Help me please. |
12/5/2011 4:33 PM | |
Posts: 510 Rating: (117) |
There are several steps to achieve the configuration you want. 1 With Com Profibus, configure the Profibus Network. Use the 545-1104 from the Master folder for the Master. In the zip file, I have included the GSD files for the 315-2PN/DP and the 315-2PN/DP V3. You will have to install the one you need in the GSD directory of Com Profibus. You should also add the bitmap to the BITMAP directory. 2. Configure the I/O for the315. Right mouse click on the 315 and select Configure. You will be adding I/O. You canconfigure up to 244 bytes of Input and 244 bytes of Outputs. 3. Export the configuration to a binary file, File > Export. Don't forget to save your configuration. 4. Using TISOFT or SoftShop merge the binary file into the I/O configuration 5. In the 545 program, you will write to the ouput area and read from the input area created by the merge to readdata from and write date to the 315. 6. In the 315 program,the data ouput from the 545 will be read in to the program from the input area you defined. Thedata you write to the output area will appear as Inputs to the 545 7. Data of lengths greater than a byte must be byte swapped since one controller is Big Endian and the other is Little Endian. The zip file includes aCom Profibus configuration with the 315 -2PN/DP firmware version prior to V3. Good Luck billwest Attachmentcomprofibus545.zip (609 Downloads) |
This contribution was helpful to1 thankful Users |
12/5/2011 9:02 PM | |
Posts: 54 Rating: (1) |
very very thanks bilwest, I will try |
12/6/2011 1:29 PM | |
Posts: 54 Rating: (1) |
Hello bilwest, Which COM PROFIBUS version is compatible with which Windows operating system? Windows 7 or windows xp running? my operating system windows7. |
12/16/2011 3:07 AM | |
Posts: 510 Rating: (117)
|
Com Profibus is old V5.1 SP2 is the latest version. I know it works with XP SP3. I have not tried it on Windows 7 billwest |
12/16/2011 4:57 AM | |
Joined: 10/7/2005 Last visit: 5/14/2024 Posts: 3005 Rating: (1048) |
Hello allen1 a quick search on that subject @ https://support.automation.siemens.comreveals the following officially supported OS's: Compatibility of COM PROFIBUS versions with Windows operating systems Just in case you want to use online functionality, the following shal help too: Applicable PROFIBUS CPs for the application ONLINE-Functions in COM PROFIBUS I hope this helps |
Cheers |
|
12/16/2011 9:34 AM | |
Posts: 54 Rating: (1) |
Thanks for the support, com profibus v5.1 software xp sp3 running |
1/27/2012 10:33 AM | |
Posts: 54 Rating: (1) |
TI545-1106 master,s7300 2pn/dp slave comm. is okey. Thanks for helps. Attachmentpic.zip (519 Downloads) |
2/26/2013 12:22 PM | |
Posts: 1 Rating: (0) |
Which COM PROFIBUS version is compatible with which Windows operating system? Windows 7 or windows xp running? my operating system windows7. |
Follow us on