4/30/2024 1:03 PM | |
Joined: 6/15/2020 Last visit: 5/20/2024 Posts: 175 Rating: (1) |
Hello, I have a unified basic hmi. I want to add a moving mixer animation here, how can I do this? Thanks. |
4/30/2024 2:02 PM | |
Joined: 2/17/2020 Last visit: 5/22/2024 Posts: 1005 Rating: (176) |
Hi, I believe you are looking for a Dynamic SVG. SIMATIC HMI WinCC Unified V19 > Managing dynamic SVG graphics |
A rating will be well appreciated. |
|
5/7/2024 6:42 AM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452)
|
Hi s27, In WinCC Unified SVG graphics itself does not support animation. In the case of dynamic SVG, you can create animation by dynamically changing the interface. However, this can have a negative effect on performance. Kind regards |
5/7/2024 6:57 AM | |
Joined: 3/30/2020 Last visit: 5/23/2024 Posts: 4531 Rating: (946) |
Perhaps there is the option of using an animated GIF via the web control item. I could not get it to work. It is not clear to me where to store the GIF file. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on