4/17/2024 5:43 PM | |
Joined: 2/17/2020 Last visit: 5/31/2024 Posts: 1008 Rating: (177) |
Hi, it is not possible to disable SNMP on the distributed IO (decentralised periphery). You can only "stop" SNMP by using two different networks. That means for example, with a S7-1200 (SNMP can be disabled with data record/ sets), you should use one interface for the connection to the internet and the other interface for the communication to the ET200SP. On the S7 1200, you can disable SNMP via data records/ sets. Please see: S7-1200 Programmable controller > Disabling SNMP |
A rating will be well appreciated. |
|
Follow us on