3/29/2023 8:10 AM | |
Joined: 9/26/2020 Last visit: 5/19/2024 Posts: 9 Rating: (0) |
Hi everybody. I'm a bit desperate. I've installed in a new server WinCC 7.5 SP2 Upd9 and Step7 V5.6 SP2 HF5. The server is: Well, when I try to start the runtime, it hangs on alarm logging and wincc explorer closes, so I did a reset_wincc.vbs to close project. I've reset alarms and tags. I've deleted .dcf and .dc* files and I've disabled and enabled MSQ and the services is running. I don't know what else to do. This is what PNDiagnose says. [snip] Please, help me. AttachmentPNDiagnose.txt (224 Downloads) |
Last edited by: Jen_Moderator at: 03/29/2023 11:24:46Diagnose added as .txt file. |
|
3/29/2023 11:09 AM | |
Joined: 7/19/2022 Last visit: 5/22/2024 Posts: 358 Rating: (61) |
Hello Macaba, I recommend you to take a look at the following FAQ: |
If this Information really helps, you could use the Rate function |
|
3/29/2023 12:28 PM | |
Joined: 9/26/2020 Last visit: 5/19/2024 Posts: 9 Rating: (0) |
Hello Murof. I created a new one too but it doesn't work. The behavior of WinCC is the same as with the other project. |
Follow us on