2/14/2024 7:35 PM | |
Joined: 1/4/2024 Last visit: 5/24/2024 Posts: 5 Rating: (0) |
Riddersholm, thank you for reaching out:) No need for a dm, maybe this post may help others aswell. After all it is a forum. I`ve translate some of the code towards English for your understanding. I hope you can help me out here so i can focus on future problems Kind Regards. This is the mask call. Basically the call is: if the alignment is greater than it should be it triggers the call. It runs from a .SPF if (AFW_Y>TOL_Y) stopre MMC("CYCLES,PICTURE_ON,POP_UP.COM,parallelism","S") M00; stopre endif This is the Mask itself. I doubt it is without flaws, but it functions and it`s my first mask:) some called variables are UGUD. [snip}
AttachmentMask.txt (86 Downloads) |
Last edited by: The Helping Hand at: 02/15/2024 10:51:37Mask added as txt-file |
|
Follow us on