1/25/2023 2:14 PM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452) |
Hi kozin, when comparing these two processors, it is noticeable that the x6414RE supports Intel® Time Coordinated Computing. Kind regards |
This contribution was helpful to1 thankful Users |
8/25/2023 12:52 AM | |
Joined: 10/30/2019 Last visit: 2/29/2024 Posts: 3 Rating: (0) |
I had a similar thought/question to Kozin. From my understanding, this intel feature about optimising real-time computing, so would this mean that the RE processor is better when you run a software controller (e.g. CPU-1507S), and the E would be better when just running WinCC RTAdv/Unifed? Regards, Brad. |
9/20/2023 11:46 AM | |
Joined: 4/18/2023 Last visit: 9/20/2023 Posts: 2 Rating: (0) |
have the same doubt regarding software controller and run time |