4/30/2016 7:31 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello In SIMATIC STEP 7 V5.5 and other SIMATIC software products released for Windows 7, the required driver for the SIMATIC USB Prommer and the PC Adapter USB are part of SIMATIC Device Drivers. A separate installation of the drivers as before via the CD supplied together with the PC Adapter resp. USB Prommer is thus no longer necessary. Please check the Settings in the PG PC interface and the connection with PLC. |
Last edited by: Navnag at: 4/30/2016 7:35:34 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
4/30/2016 7:54 AM | |
Joined: 3/28/2015 Last visit: 5/10/2024 Posts: 721 Rating: (213) |
Hello, Kindly find the attached file. AttachmentS7_Downloading_ Uploading.pdf (916 Downloads) |
Eng.Mohamed Ibrahim |
|
5/1/2016 8:50 AM | |
Joined: 3/17/2013 Last visit: 12/25/2023 Posts: 480 Rating: (43) |
Also take care that you are connecting on CPU to MPI port. Regards, Vijay |
5/2/2016 6:18 AM | |
Posts: 8 Rating: (0) |
Dear Mr.Duris, Please find the attached picture for pc adapter. Thanks Mani |
5/2/2016 6:22 AM | |
Posts: 8 Rating: (0) |
Dear Mr.Smith, In my laptop I have installed Simatic manager software only.I don't have microwin software. Thanks Mani |
5/2/2016 6:50 AM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836)
|
Hello, To connect to S7-200, you should install MicroWin V4.0 SP9. This version is tested for your OS. STEP7 MicroWIN V4.0 SP8 and SP9 To connect to S7-300/400. Your Step 7 should work. Hope this helps. AttachmentSTEP-7-(STEP-7-Professional)_V5.5_compatibility-list_en_2016-04-25.zip (285 Downloads) |
Last edited by: Ayman Elotaify at: 5/2/2016 6:53:05 AMLast edited by: Ayman Elotaify at: 5/2/2016 6:59:30 AMAyman Elotaify |
|
5/2/2016 7:25 AM | |
Posts: 8 Rating: (0) |
Dear Mr.Ankurgamit, Please find the attached picture which is shown on my laptop's device manager page. Thanks |
Follow us on